Post Go back to editing

RMS-to-DC for Sound Pressure Level measurement

Hi,

I want to measure the RMS value of a microphone's output voltage (to get the SPL value in dB).

I see a lot of RMS-to-DC IC seem to do that but I am wondering :

At a given moment, if I read the output of the RMS chip (on an ADC), is the RMS (the average/mean part) calculated on the last 10ms ? 100ms ? 1sec ?

In other words, I want to read the RMS value every second. So I want it to be representative of the last second that just passed not the last 10ms.

How is it related to the "settling time" parameter (if it is) ?

Best regards,

V.

Parents Reply Children
No Data