Post Go back to editing

About connection of ADAU1978 and ADXL316

Thread Summary

The user inquired about connecting an ADXL316 accelerometer to an ADAU1978 Audio-ADC for sampling microphone and accelerometer outputs. The final answer indicates that the ADAU1978's narrow single-end input voltage range prevents it from being directly connected to the ADXL316. The thread is closed with no additional solutions provided.
AI Generated Content

Hi all

We are in a new project of the ANC.

We are planning to sample the output of the microphone and the accelerometers to the Audio-ADC.

Target devices are ADAU1978 and ADXL316.

Is it can be realized?

Please let us know if there is a concern.

Best Regards

AimPoint