I want to configure the ADAU1761 so that the audio can input from the mic pin......
ADAU1761
Production
The ADAU1761 is a low power, stereo audio codec with integrated digital audio processing that supports stereo 48 kHz record and playback at 14 mW from...
Datasheet
ADAU1761 on Analog.com
I want to configure the ADAU1761 so that the audio can input from the mic pin......
Hello starbuck666,
This is explained in the datasheet in the section labeled "Digital Microphone Input". Page 31. If you are using our evaluation board then you must also change a jumper to change the pin from a jackdetect function to connect to the digital mic header on the eval board. It is jumper J7 and the setting is written on the silk screen of the PCB.
Dave T