SigmaStudio Network Utility for Linux seems to be outdated

SigmaStudio Network Utility for Linux seems to be outdated.  Based on debugging I have made, the protocol has changed in some stage.  Is there any working code available anywhere?  The latest version here https://github.com/analogdevicesinc/sigma-tcp doesn't really work.

I have understanding on the writing commands but register read command is mystery as the latest information on the response packet format doesn't seem to work.

Parents
  • Yes and no and both.  Clearly SigmaStudio Network Utility for Linux doesn't work as.  If it did, I could deduce the protocol from it.  And the two communicate with each other so they should be in sync.  And this would be very useful because it would make it much easier to implement in device development.  In ideal case, if the device has Linux or any CPU with real time communication to a supporting Linux machine, no extra hardware would be necessary.

Reply
  • Yes and no and both.  Clearly SigmaStudio Network Utility for Linux doesn't work as.  If it did, I could deduce the protocol from it.  And the two communicate with each other so they should be in sync.  And this would be very useful because it would make it much easier to implement in device development.  In ideal case, if the device has Linux or any CPU with real time communication to a supporting Linux machine, no extra hardware would be necessary.

Children
No Data