Hi
My customers chose the AD 1854 as an alternative to the AD 1852, which became an EOL.
The customer buffered the audio output of the AD 1854 and the customer gave control signals and data to the AD 1854 in the same way as the AD 1852.
However, AD 1854 did not behave similarly.
I doubt the MASTER CLOCK AUTODIVIDE FEATURE circuit.
Because the problem seems not to be an audio signal.
We are giving a burst clock to the AD 1854.
The burst clock is accepted by the data sheet, just like the AD 1852.
Is it wrong to give the same control signal to the AD 1854 and AD 1852?
Best regards