I wonder if Analog Devices provides an USB to I2S audio bridge? Either as one component or as a combination. It should handle USB 2, PCM 352/384 32 bit and DSD128 to PCM 176. On the other end there is a DSP (ADAU1467) running at 192/32. Audio direction is only from USB host to DSP. Since the DSP is running at 192, the bridge must be able to perform the sample rate conversion of the PCM stream down to 176/192.
I have done some searching and as far as I can see I will need to source the USB interface from other supplier but eventually there is some Analog Device solution that will be able to take care of the down sampling to match the sample rate of the DSP. Am I correct?
No docs yet.
These specs are preliminary and subject to change, but::
Sorry about that.
Yes. It will support USB Audio 2.0. It will include a configuration utility for configuring the sample rate, number of channels, data and clock pin formatting, etc. The utility will store…
Markus,
This project was delayed due to circumstances beyond our control, but it is still moving forward. I am evaluating the latest hardware received just last week. The circuit is finalized, but we will…
Yes. It will support USB Audio 2.0. It will include a configuration utility for configuring the sample rate, number of channels, data and clock pin formatting, etc. The utility will store the configuration, and the board will continue operating with that formatting until the utility is run again. Since SigmaStudio is only supported on Windows, it is not unlikely that we will official support this utility on any other platform. However, officially unsupported versions may be available. Once the board is configured in the desired operating mode however, I would expect it to record and play on any platform that supports UAC2. The USBi functionality will, however, only work within SigmaStudio (and therefore only on Windows).
Is it possible you could share who is the consulting partner that is developing this board?