SSM2142
Obsolete
The SSM2142 is an integrated differential-output buffer amplifier that converts a single-ended input signal to a balanced output signal pair with high...
Datasheet
SSM2142 on Analog.com
SSM2143
Obsolete
The SSM2143 is an integrated differential amplifier intended to receive balanced line inputs in audio applications requiring a high level of immunity from...
Datasheet
SSM2143 on Analog.com
Hi there,
With the SSM2142 and SSM2143 going end of life we're looking for an alternate set of audio line driver and receiver chips.
We need to drive up to 5Vrms into a 600 Ohm load, and our receiver should be 600 Ohms and capable of receiving up to 5Vrms. Input and output voltages to the system will be abut 1Vrms.
What can we use in their place?
Regards,
Glenn
I posted this question in Audio, and they suggested I take it to the amplifiers forum.
I posted this question in Audio, and they suggested I take it to the amplifiers forum.