ADV7535

Hi Sir,

We are testing Rockchip RK3399 platform and ADV7535 MIPI to HDMI converter solution now.

We imported script file as blow into ADV7535,than enabled internal testing pattern x55 (TPG_pattern_sel), it seems color bar output function okay.

But If I changed MIPI routing input, it can’t see output in the monitor.

May I have your help for any setting should be check?

BTW, We also tried this script file successful in the NXP platform + ADV7535.

 

------------------------------------------------------------------------------------------------------------------------------------

:1920 x 1080p-60Hz DSI 24BPP - 4 x DSI Lanes - RGB Out:

include this "01 Power Up and Initialisation" "01-02 Power"

include this "01 Power Up and Initialisation" "01-03 Initialisation (Fixed) Registers"

include this "02 DSI Video Input Mode" "02-04 4 x DSI Lanes"

include this "02 DSI Video Input Mode" "02-05 DSI Pixel Clock Divider - Automatic (default)"

include this "03 Internal Timing Generator" "03-01 Enable Internal Timing Generator (default)"

include this "03 Internal Timing Generator" "03-04 1920 x 1080p 60Hz"

include this "03 Internal Timing Generator" "03-03 Reset Internal Timing Generator"

include this "04 Video Output Mode" "04-01 HDMI Output"

include this "09 AVI Info-frame" "09-03 AVI Infoframe - RGB - 16-9 Aspect Ratio"

include this "04 Video Output Mode" "04-04 GC Packet Enable"

include this "04 Video Output Mode" "04-06 GC Colour Depth - 24 Bit"

include this "04 Video Output Mode" "04-09 Down Dither Output Colour Depth - 8 Bit (default)"

include this "05 Audio Setup" "05-02 Audio Data and Clock and CEC Not Gated"

include this "05 Audio Setup" "05-07 N Value (6144) for 48kHz Audio"

include this "05 Audio Setup" "05-12 Select I2S Audio (default)"

include this "05 Audio Setup" "05-16 I2S Enable (default)"

include this "05 Audio Setup" "05-18 I2S Sampling Frequency 48kHz"

include this "07 CEC" "07-01 CEC Power Mode - Always Active"

include this "04 Video Output Mode" "04-03 HDMI Output Enable"

End

------------------------------------------------------------------------------------------------------------------------------------

Top Replies