Post Go back to editing

SSM2143 Audio Differential Line Receiver

I would like to use the SSM2143 Differential Line Receiver in a Dual Channel Audio Interface and A/D Converter, but the available supply voltages are lower than the +/- 15 V indicated by the datasheet.

I would be very grateful if somebody could tell me what are the performances (max. Input Level, Distortion, Noise) of the device when powered with +/- 10 V, considering an output load between 2 and 10 kOhm, and a -6dB Gain configuration.

Thank you very much in advance!

Alberto

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.