Need suggestions for correct full-scale ADC values

Hello,

This question is about giving the correct value to the ADC input resistor of ADAU1701. However, since it is more of a general audio application question, I thought of posting it here to get suggestions from a wider audience.

I will be using the ADAU1701 SigmaDSP processor in home application as well as in Pro applications.

Will it be correct to assume an input full scale value of 0.316V (-10dbV) for home/ domestic use (with Media players, STB audio output etc.) and 1.228V (+4dbU) for PRO use (Mike/ AUX/ DJ mixer)?

Do suggest you you have any other views/ opinions.

Thanks in advance!!

Note: Since the processor already has a 2k resistor internally, I'll have to re-adjust the input full scale for Home



SigmaDSP specific note added at the end
[edited by: KKSL at 5:07 PM (GMT 0) on 11 Feb 2019]
Parents Reply Children