KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
AD1896
Production
The AD1896 is a sample rate converter; it is second generation and 24-bit, high-performance, single-chip, and asynchronous. Based upon Analog Devices experience...
Datasheet
AD1896 on Analog.com
AD1865
Obsolete
The AD1865 is a complete, dual 18-bit DAC offering excellent THD+N and SNR while requiring no external components. Two complete signal channels are included...
AD1865 on Analog.com
Hi,
I am working on non-oversampling DAC for CD standard 44.1/16, and looking for simple way of re-clocking I2S input format and realign it to 18-bit EIAJ for AD1865NK. Is there way to use AD1896 for this? I see that there is bypass mode (I don't want to change sample rate), but it is not clear to me, if in this mode AD1896 output signals (SDATA, SCLK, LRCLK) are (re)clocked by external MCLK_I.
Regards,
josip