Hi all,
How about is the VIN Absolute Maximum Ratings ?
Is it correct, –0.3 V to AVDD + 0.3 V ?
Best regards,
sss
Hello sss@jpn,
I see that it is missing from the absolute maximum section of the datasheet. The standard specification for most of our devices is what you stated, -0.3 V to AVDD + 0.3 V. This comes from…
I see that it is missing from the absolute maximum section of the datasheet. The standard specification for most of our devices is what you stated, -0.3 V to AVDD + 0.3 V. This comes from the ESD protection devices on the pins. Since the digital pins have this specification I can assume the same, or similar, ESD devices were used on the analog pins as well as the digital pins.
So I say you are correct. That is a common and safe assumption.
Dave T