ADAU1761 record and playback problem

Hi,everyone

   I am a picozed sdr2 + fmc board user, and I wan't get pcm data stream and play it back via adau1761,the C code lists as follows:

//--------------------------------------------------------------------

record.c

/*

Example 4 - Simple sound recording

This example reads from the default PCM device
and writes to standard output for 5 seconds of data.

*/

/* Use the newer ALSA API */
#define ALSA_PCM_NEW_HW_PARAMS_API

#include <alsa/asoundlib.h>

int main() {
long loops;
int rc;
int size;
snd_pcm_t *handle;
snd_pcm_hw_params_t *params;
unsigned int val;
int dir;
snd_pcm_uframes_t frames;
char *buffer;

/* Open PCM device for recording (capture). */
rc = snd_pcm_open(&handle, "default",
SND_PCM_STREAM_CAPTURE, 0);
if (rc < 0) {
fprintf(stderr,
"unable to open pcm device: %s\n",
snd_strerror(rc));
exit(1);
}

/* Allocate a hardware parameters object. */
snd_pcm_hw_params_alloca(&params);

/* Fill it in with default values. */
snd_pcm_hw_params_any(handle, params);

/* Set the desired hardware parameters. */

/* Interleaved mode */
snd_pcm_hw_params_set_access(handle, params,
SND_PCM_ACCESS_RW_INTERLEAVED);

/* Signed 16-bit little-endian format */
snd_pcm_hw_params_set_format(handle, params,
SND_PCM_FORMAT_S16_LE);

/* Two channels (stereo) */
snd_pcm_hw_params_set_channels(handle, params, 2);

/* 44100 bits/second sampling rate (CD quality) */
val = 44100;
snd_pcm_hw_params_set_rate_near(handle, params,
&val, &dir);

/* Set period size to 32 frames. */
frames = 32;
snd_pcm_hw_params_set_period_size_near(handle,
params, &frames, &dir);

/* Write the parameters to the driver */
rc = snd_pcm_hw_params(handle, params);
if (rc < 0) {
fprintf(stderr,
"unable to set hw parameters: %s\n",
snd_strerror(rc));
exit(1);
}

/* Use a buffer large enough to hold one period */
snd_pcm_hw_params_get_period_size(params,
&frames, &dir);
size = frames * 4; /* 2 bytes/sample, 2 channels */
buffer = (char *) malloc(size);

/* We want to loop for 5 seconds */
snd_pcm_hw_params_get_period_time(params,
&val, &dir);
loops = 5000000 / val;

while (loops > 0) {
loops--;
rc = snd_pcm_readi(handle, buffer, frames);
if (rc == -EPIPE) {
/* EPIPE means overrun */
fprintf(stderr, "overrun occurred\n");
snd_pcm_prepare(handle);
} else if (rc < 0) {
fprintf(stderr,
"error from read: %s\n",
snd_strerror(rc));
} else if (rc != (int)frames) {
fprintf(stderr, "short read, read %d frames\n", rc);
}
rc = write(1, buffer, size);
if (rc != size)
fprintf(stderr,
"short write: wrote %d bytes\n", rc);
}

snd_pcm_drain(handle);
snd_pcm_close(handle);
free(buffer);

return 0;
}

//--------------------------------------------------------------------

playback.c

/*

Example 3 - Simple sound playback

This example reads standard from input and writes
to the default PCM device for 5 seconds of data.

*/

/* Use the newer ALSA API */
#define ALSA_PCM_NEW_HW_PARAMS_API

#include <alsa/asoundlib.h>

int main() {
long loops;
int rc;
int size;
snd_pcm_t *handle;
snd_pcm_hw_params_t *params;
unsigned int val;
int dir;
snd_pcm_uframes_t frames;
char *buffer;

/* Open PCM device for playback. */
rc = snd_pcm_open(&handle, "default",
SND_PCM_STREAM_PLAYBACK, 0);
if (rc < 0) {
fprintf(stderr,
"unable to open pcm device: %s\n",
snd_strerror(rc));
exit(1);
}

/* Allocate a hardware parameters object. */
snd_pcm_hw_params_alloca(&params);

/* Fill it in with default values. */
snd_pcm_hw_params_any(handle, params);

/* Set the desired hardware parameters. */

/* Interleaved mode */
snd_pcm_hw_params_set_access(handle, params,
SND_PCM_ACCESS_RW_INTERLEAVED);

/* Signed 16-bit little-endian format */
snd_pcm_hw_params_set_format(handle, params,
SND_PCM_FORMAT_S16_LE);

/* Two channels (stereo) */
snd_pcm_hw_params_set_channels(handle, params, 2);

/* 44100 bits/second sampling rate (CD quality) */
val = 44100;
snd_pcm_hw_params_set_rate_near(handle, params,
&val, &dir);

/* Set period size to 32 frames. */
frames = 32;
snd_pcm_hw_params_set_period_size_near(handle,
params, &frames, &dir);

/* Write the parameters to the driver */
rc = snd_pcm_hw_params(handle, params);
if (rc < 0) {
fprintf(stderr,
"unable to set hw parameters: %s\n",
snd_strerror(rc));
exit(1);
}

/* Use a buffer large enough to hold one period */
snd_pcm_hw_params_get_period_size(params, &frames,
&dir);
size = frames * 4; /* 2 bytes/sample, 2 channels */
buffer = (char *) malloc(size);

/* We want to loop for 5 seconds */
snd_pcm_hw_params_get_period_time(params,
&val, &dir);
/* 5 seconds in microseconds divided by
* period time */
loops = 5000000 / val;

while (loops > 0) {
loops--;
rc = read(0, buffer, size);
if (rc == 0) {
fprintf(stderr, "end of file on input\n");
break;
} else if (rc != size) {
fprintf(stderr,
"short read: read %d bytes\n", rc);
}
rc = snd_pcm_writei(handle, buffer, frames);
if (rc == -EPIPE) {
/* EPIPE means underrun */
fprintf(stderr, "underrun occurred\n");
snd_pcm_prepare(handle);
} else if (rc < 0) {
fprintf(stderr,
"error from writei: %s\n",
snd_strerror(rc));
} else if (rc != (int)frames) {
fprintf(stderr,
"short write, write %d frames\n", rc);
}
}

snd_pcm_drain(handle);
snd_pcm_close(handle);
free(buffer);

return 0;
}

I want do a small test is that when I say something from mic,and the headphone would play it immediately.  

So, after compiled the two .c file, I use the cmd line "./record | ./playback" in the ubuntu terminial on picozed development kit to run both of them. The terminal print "under run" string over and over again, and I can hear nothing from headphone when I talk to mic.

But when I use the same code and same operation on my PC, It works very well.

So,can anyone give some tips for me, thanks!

lin-

(The two .c file as a attachement of this topic.)@@@

attachments.zip