ad1938: FAQ

  • Created
  • Updated
Was this helpful?
  • Sample rate lower than 32KHz

    Q I would like to use the chip below 32KHz sample rate, how should I configure it? A The default condition would be a 12.288 MHz crystal (48 kHz * 256) and the PLL using MCLK as its input source…
  • Using LRCLK as PLL input

    Q I use the AD1938 in slave mode and provide the ALRCLK externally. I would like to know if I need to configure the PLL INPUT register to set the ALRCLK as the PLL input, whether I still need to provide…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.