Post Go back to editing

June 2025 StudentZone Quiz Solution

Question 1: What is the main function of a Peltz oscillator?

 

Answer 1:

The Peltz oscillator is used to generate sinusoidal signals and is especially suited for high frequency applications. Its main function is to provide a stable oscillation with low distortion, typically in RF or VHF circuits.

 

Question 2: The Peltz oscillator is a variation of which oscillator?

 

Answer 2:

The Peltz oscillator is a variation of the Colpitts oscillator, similar to the Clapp design. However, it introduces a slightly different configuration to improve performance characteristics such as frequency stability and output amplitude.

 

Question 3: Which component configuration differentiates the Peltz oscillator from the Colpitts and Clapp oscillators?

 

Answer 3:

The Peltz oscillator often uses a different feedback network and biasing arrangement to improve performance. One distinguishing feature is that it may incorporate a tuned transformer or tapped inductor to influence the oscillation conditions and improve stability or impedance matching.

 

Question 4: When is a Peltz oscillator preferred over other LC oscillators like Colpitts or Clapp?

 

Answer 4:

The Peltz oscillator is preferred in high frequency circuits that require minimal harmonic distortion and good amplitude stability. It’s also useful where impedance transformation or isolation is needed due to its transformer-based variations.


See the article:

https://www.analog.com/en/resources/analog-dialogue/studentzone/studentzone-june-2025.html