Question 1:
What are the components commonly used to tune amplifiers when op amps are not suitable for high frequency requirements?
Answer 1:
LC (parallel inductor-capacitor) resonant circuits are commonly used to tune amplifiers when op amps are not suitable for high frequency requirements.
Question 2:
What happens to the impedance of a parallel resonant circuit at its resonant frequency, and how does this affect the voltage gain of a common emitter amplifier?
Answer 2:
At the resonant frequency, the impedance of a parallel resonant circuit is extremely high. When a common emitter amplifier is operated at this frequency, the collector load impedance is also at its maximum value, resulting in the maximum voltage gain of the amplifier.
Question 3:
What is the primary function of the high-pass filter, and how does it affect the amplifier’s input signal?
Answer 3:
The primary function of the high-pass filter is to filter out low frequency components from the input signal. It allows higher frequencies to pass through, improving the amplifier’s performance for certain applications.