Post Go back to editing

December 2023 StudentZone Quiz Solution

Question 1:

Use the formula for the self-resonance frequency to calculate the value for the turn-to-turn parasitic capacitance of the inductor used in your experimental setup.

Answer 1:

The value of the turn-to-turn parasitic capacitance of the inductor used in the experimental setup can be computed as follows:

Given the values:

L = 100 μH

fSR = 5 MHz

We obtain the value of Cparasitic ≈ 1.275 × 10−15 F ≈ 1.275 fF.

Edit Notes

_
[edited by: AnnLaz at 3:52 PM (GMT -5) on 4 Dec 2023]