Question 1:
Using the values and formulas provided in the laboratory directions compute the following parameters:
Answer 1:

IF = 7mA

Fc1 = 0.33Hz

Fc2 = 3.3Hz

Fc3 = 3.3Hz

AV = - 470
Question 2:
What parameters change if R5 is modified?
Answer 2:
If R5 is modified, this will affect the gain of the third stage amplifier.
Question 3:
What parameters change if R6 is modified?
Answer 3:
If R6 is modified, this will affect both the gain of the third stage amplifier and the cut-off frequency of the third stage low-pass filter.
Reg. Q1: You get IF=7mA with VF = 1,7V. When I study the datasheet, how can I be sure, the LED wil work at 7mA? The IF/VF diagram starts at IF=10mA, VF~1,2V . All Optical parameters refers to 20mA. It feels like R1 is a slightly to high for VP=5V.
Reg. Q1: You get IF=7mA with VF = 1,7V. When I study the datasheet, how can I be sure, the LED wil work at 7mA? The IF/VF diagram starts at IF=10mA, VF~1,2V . All Optical parameters refers to 20mA. It feels like R1 is a slightly to high for VP=5V.