Question 1:
Can you derive the sensitivity in mV/ºC you measured from the diode equation?
Answer 1:
We can obtain the sensitivity in mV/ºC measured from the diode equation by taking into account the following values from the activity:
Tref=25ºC
Vref=-6.953mV (obtained from the measurement presented in Figure 3)
Vtemp=7.879mV (obtained from the measurement presented in Figure 4)
The temperature of the sensor can be obtained using the following formula:

The sensitivity of the sensor is computed as follows:

Question 2:
What is the purpose of the reference diode in this configuration?
Answer 2:
The reference diode serves as the temperature reference maintained at a constant temperature, considered as room temperature (25º C) for the experiments.
The sensitivity of the sensor is computed as follows: