Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

How-To use EVAL-ADICUP3029 / EV-COG-AD3029 with emIDE

The official supported toolchain - Cross-Core-Embedded-Studio - for the EVAL-ADICUP3029 and EV-COG-AD3029 boards which is based on Eclipse, is working well.

But some people, including myself, like to use a simpler and easier to use approach for small Bare-Metal projects - as for example I've written in How to - ADuCM3029 with simple and free Open Source Tools? For this I used at that time a J-Link Debug Probe from SEGGER, which can also be used with those two boards.


But the big advantage of the EVAL-ADICUP3029 and EV-COG-AD3029 boards is that they already come with an integrated OpenOCD based Debug Probe onboard.

This time I have selected the emIDE on Windows for a small tutorial on How-To use it with that boards.

Attached here is a quick tutorial, the required OpenOCD driver and a basic example project for each of the boards.

Comments
Anonymous
Related