UART data transfer speed & OS support of ADuCM4050

Hi Sir,

I am using ADuCM4050 in my project. I have below 2 queries:-

  1. What is the data transfer speed of UART in controller ?
  2. Which operating system does this controller support ?

Thanks in advance!

Parents
  • Hi

    1. I've successfully used the ADuCM4050 UART at 1.5Mbaud on many projects. There are configutration examples for 3Mbaud and 6Mbaud as well, but I've not tried those.

    2. the UART peripheral and associated drivers are operating system agnostic. You should be able to use the UART from within any RTOS that otherwise works on the ADuCM4050. Likewise you should be able to communicate via the UART to any other system with a UART regardless of the OS running on that system.

    -Jared

Reply
  • Hi

    1. I've successfully used the ADuCM4050 UART at 1.5Mbaud on many projects. There are configutration examples for 3Mbaud and 6Mbaud as well, but I've not tried those.

    2. the UART peripheral and associated drivers are operating system agnostic. You should be able to use the UART from within any RTOS that otherwise works on the ADuCM4050. Likewise you should be able to communicate via the UART to any other system with a UART regardless of the OS running on that system.

    -Jared

Children
No Data