Hi support team,
I use IAR, and i got many board ( all exactly the same ) with sensors control by an ADUCM3029. All cards work very well, but two of them give me an error when i want to flash the code on the board :
"The flash loader program reported an error"
"A fatal error has occurred, the debugger will terminate"
I use a J-Link debugger, and i checked on J-link commander software ( and also manualy) the voltage of different pin, and the supply voltage, and all is correct, and the device is identified correctly.
I also tried to erase flash memory, but i didn't solve the problem.
The following line are my error message on IAR worspace :
Tue Aug 01, 2017 16:36:01: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\arm\config\flashloader\AnalogDevices\FlashADUCM3029.mac Tue Aug 01, 2017 16:36:01: JLINK command: ProjectFile = C:\Users\avouaill\Desktop\workspace\Puck_project_debug_Beacon_Juillet_2017\Puck_project\settings\second_test_Debug.jlink, return = 0 Tue Aug 01, 2017 16:36:01: Device "ADUCM3029" selected. Tue Aug 01, 2017 16:36:01: DLL version: V6.10c, compiled Sep 28 2016 18:45:15 Tue Aug 01, 2017 16:36:01: Firmware: J-Link Lite-ADI Rev.1 compiled Jan 7 2013 17:58:04 Tue Aug 01, 2017 16:36:01: Selecting SWD as current target interface. Tue Aug 01, 2017 16:36:01: JTAG speed is initially set to: 1000 kHz Tue Aug 01, 2017 16:36:01: Found SWD-DP with ID 0x2BA01477 Tue Aug 01, 2017 16:36:01: AP-IDR: 0x24770011, Type: AHB-AP Tue Aug 01, 2017 16:36:01: Found Cortex-M3 r2p1, Little endian. Tue Aug 01, 2017 16:36:01: FPUnit: 2 code (BP) slots and 0 literal slots Tue Aug 01, 2017 16:36:01: CoreSight components: Tue Aug 01, 2017 16:36:01: ROMTbl 0 @ E00FF000 Tue Aug 01, 2017 16:36:01: ROMTbl 0 [0]: FFF0F000, CID: B105E00D, PID: 000BB000 SCS Tue Aug 01, 2017 16:36:01: ROMTbl 0 [1]: FFF02000, CID: B105E00D, PID: 003BB002 DWT Tue Aug 01, 2017 16:36:01: ROMTbl 0 [2]: FFF03000, CID: B105E00D, PID: 002BB003 FPB Tue Aug 01, 2017 16:36:01: Hardware reset with strategy 3 was performed Tue Aug 01, 2017 16:36:01: Initial reset was performed Tue Aug 01, 2017 16:36:02: -I- execUserFlashInit! Tue Aug 01, 2017 16:36:02: 904 bytes downloaded (18.78 Kbytes/sec) Tue Aug 01, 2017 16:36:02: Loaded debugee: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\arm\config\flashloader\AnalogDevices\FlashADUCM3029.out Tue Aug 01, 2017 16:36:02: Target reset Tue Aug 01, 2017 16:36:02: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\arm\config\flashloader\AnalogDevices\FlashADUCM3029.mac Tue Aug 01, 2017 16:36:02: The flash loader program reported an error.
Any idea let me know,
Best regards,
Florent