Post Go back to editing

Error "The flash loader program reported an error"

Hi support team, 

I use IAR, and i got many board ( all exactly the same ) with sensors control by an ADUCM3029. All cards work very well, but two of them give me an error when i want to flash the code on the board :

"The flash loader program reported an error"

"A fatal error has occurred, the debugger will terminate"

I use a J-Link debugger, and i checked on J-link commander software ( and also manualy)  the voltage of different pin, and the supply  voltage, and all is correct, and the device is identified correctly.

I also tried to erase flash memory, but i didn't solve the problem.

The following line are my error message on IAR worspace :

Tue Aug 01, 2017 16:36:01: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\arm\config\flashloader\AnalogDevices\FlashADUCM3029.mac  Tue Aug 01, 2017 16:36:01: JLINK command: ProjectFile = C:\Users\avouaill\Desktop\workspace\Puck_project_debug_Beacon_Juillet_2017\Puck_project\settings\second_test_Debug.jlink, return = 0  Tue Aug 01, 2017 16:36:01: Device "ADUCM3029" selected.  Tue Aug 01, 2017 16:36:01: DLL version: V6.10c, compiled Sep 28 2016 18:45:15  Tue Aug 01, 2017 16:36:01: Firmware: J-Link Lite-ADI Rev.1 compiled Jan  7 2013 17:58:04  Tue Aug 01, 2017 16:36:01: Selecting SWD as current target interface.  Tue Aug 01, 2017 16:36:01: JTAG speed is initially set to: 1000 kHz  Tue Aug 01, 2017 16:36:01: Found SWD-DP with ID 0x2BA01477  Tue Aug 01, 2017 16:36:01: AP-IDR: 0x24770011, Type: AHB-AP  Tue Aug 01, 2017 16:36:01: Found Cortex-M3 r2p1, Little endian.  Tue Aug 01, 2017 16:36:01: FPUnit: 2 code (BP) slots and 0 literal slots  Tue Aug 01, 2017 16:36:01: CoreSight components:  Tue Aug 01, 2017 16:36:01: ROMTbl 0 @ E00FF000  Tue Aug 01, 2017 16:36:01: ROMTbl 0 [0]: FFF0F000, CID: B105E00D, PID: 000BB000 SCS  Tue Aug 01, 2017 16:36:01: ROMTbl 0 [1]: FFF02000, CID: B105E00D, PID: 003BB002 DWT  Tue Aug 01, 2017 16:36:01: ROMTbl 0 [2]: FFF03000, CID: B105E00D, PID: 002BB003 FPB  Tue Aug 01, 2017 16:36:01: Hardware reset with strategy 3 was performed  Tue Aug 01, 2017 16:36:01: Initial reset was performed  Tue Aug 01, 2017 16:36:02: -I- execUserFlashInit!  Tue Aug 01, 2017 16:36:02: 904 bytes downloaded (18.78 Kbytes/sec)  Tue Aug 01, 2017 16:36:02: Loaded debugee: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\arm\config\flashloader\AnalogDevices\FlashADUCM3029.out  Tue Aug 01, 2017 16:36:02: Target reset  Tue Aug 01, 2017 16:36:02: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\arm\config\flashloader\AnalogDevices\FlashADUCM3029.mac  Tue Aug 01, 2017 16:36:02: The flash loader program reported an error. 

Any idea let me know,

Best regards,

Florent

Top Replies

Parents Reply Children
No Data