ADuCM4050: Using the UART boot routine from my application

Hi,

I want to be able to use Analog Devices's UART bootloader routine that is in the boot kernel of the ADuCM4050, from within my code, without the need to reset the micro-controller and force "0" on GPIO17.

Can you provide the address to which my code should jump to, immediately after checking the GPIO17 and deciding that it should continue as bootloader?

Thanks,

Kobi