I'm trying to build a project that transmits data via xbee in regular interval of time. So for this I used the uart and rtc functions of ev-cog-ad3029lz. This program works fine in debug mode. When trying to build in release mode it gives this error. I want my project work stand-alone without being connected to the pc. What should I do.?
Hi,
Please read this FAQ it will help you on working with stand alone mode.
Regards,
Jeric
Can you check CrossCore GCC ARM Embedded Assembler, CrossCore GCC ARM Embedded C Compiler and CrossCore GCC ARM C++ Compiler settings All options if you have define -mcpu=cortex-m3. If not, define it to…
You have to configure your linker file to put the data on retained RAM region, goto folder name RTE>>device>>aducm3029 and look for aduc3029.ld change both .data and .bss to DSRAM_A
-jeric
Sir I did replace common.h file but nothing happened still getting the same error
please refer to the image attached.
this where my program gets stuck in release mode.
Can you share your full project?