Using FreeRTOS on EV-COG-AD4050LZ

Hi,

I want to run FreeRtos on EV-COG-AD4050LZ. I downloaded the software from here and followed the user guide.

When I try to build and run the RTOSDemo example, the project builds without errors but I get the following errors while flashing:

Fri Apr 26, 2019 15:21:37: The downloaded program doesn't seem to match the expected memory layout of the target system:
Fri Apr 26, 2019 15:21:37: There are linked memory segments outside known memory areas.
Fri Apr 26, 2019 15:21:37: Memory is specified as follows:
Fri Apr 26, 2019 15:21:37: 0x00000000 - 0x1FFFFFFF ROM/Flash
Fri Apr 26, 2019 15:21:37: 0x20000000 - 0x21FFFFFF RAM
Fri Apr 26, 2019 15:21:37: 0x22000000 - 0x23FFFFFF RAM
Fri Apr 26, 2019 15:21:37: 0x40000000 - 0x41FFFFFF Uncached/SFR
Fri Apr 26, 2019 15:21:37: 0x42000000 - 0x43FFFFFF Uncached/SFR
Fri Apr 26, 2019 15:21:37: 0xE0000000 - 0xFFFFFFFF Uncached/SFR
Fri Apr 26, 2019 15:21:37: Segments are linked as follows:
Fri Apr 26, 2019 15:21:37: 0x00000000 - 0x0000015F ROM/Flash
Fri Apr 26, 2019 15:21:37: 0x00000180 - 0x0000019F ROM/Flash
Fri Apr 26, 2019 15:21:37: 0x000007FC - 0x000007FF RAM
Fri Apr 26, 2019 15:21:37: 0x00000800 - 0x00006BB3 ROM/Flash
Fri Apr 26, 2019 15:21:37: 0x20000000 - 0x20004F83 RAM
Fri Apr 26, 2019 15:21:37: 0x20053800 - 0x20053FFF RAM
Fri Apr 26, 2019 15:21:37: Download error at 0x00000000: downloading into non-writable memory.
Fri Apr 26, 2019 15:21:37: Download error at 0x00000000: memory write failed.
Fri Apr 26, 2019 15:21:40: IAR Embedded Workbench 8.20.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\bin\armproc.dll)
Fri Apr 26, 2019 15:21:41: Loading the CMSIS-DAP driver

I am using IAR v8.20.