Terminated OpenOCD Process with EV-COG-AD4050LZ

Hi,all.

I am using EV-COG-405Z in the following environment, currently.

IDE:CrossCore Embedded Studio
IDE version:2.8.44.201803091352
DFP:AnalogDevices.ADuCM4x50_DFP.3.2.0
BSP:AnalogDevices.EV-COG-AD4050LZ_BSP.3.1.0
CMSIS:ARM.CMSIS.5.1.1

I copied and executed Blinky_example (EV - COG - AD 4050 LZ) from CMSIS Pack Manager.
After that, the following message is displayed on the console and the program is not executed.

Open On-Chip Debugger (Analog Devices CCES 2.8.0 OpenOCD 0.9.0-g5030ad7) 0.9.0
Licensed under GNU GPL v2
Report bugs to <processor.tools.support@analog.com>
0
Info : select transport "swd"
adapter speed: 1000 kHz
cortex_m reset_config sysresetreq
Info : CMSIS-DAP: SWD Supported
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : CMSIS-DAP: FW Version = 1.0
Info : SWCLK/TCK = 0 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 1000 kHz
in procedure 'init'
in procedure 'ocd_bouncer'

What are the possible causes of this problem?

Thanks

Parents Reply Children
No Data