Linker file configuration on aducm4050

Hi everybody!

I use EV COG AD4050LZ eval board. 
I need to increase my STACK size inside my Linker file and i don't know how to do this. 

Here is my standart linker file for ADUCM4050

/*###ICF### Section handled by ICF editor, don't touch! ****/
/*-Editor annotation file-*/
/* IcfEditorFile="$TOOLKIT_DIR$\config\ide\IcfEditor\cortex_v1_0.xml" */

/*-Sizes-*/
define symbol __ICFEDIT_size_cstack__ = 2K;
define symbol __ICFEDIT_size_heap__   = 80K;

/**** End of ICF editor section. ###ICF###*/

define memory mem with size        = 4G;

// symbols
define symbol USE_PARITY = 1;

define symbol FLASH                               = 0x00000000;  // flash address
define symbol FLASH_SIZE                          = 508K;        // flash size (excluding Protected Key Storage)
define symbol FLASH_PAGE_SIZE                     = 2K;          // 2k flash page size
define symbol PAGE0_ROM_START                     = 0x1A0;

define symbol START_OF_SEC_HDR                    = 0x00000180;  // security header


// user-selectable SRAM mode
define symbol USER_SRAM_MODE = 0;

// RAM bank sizes sizes are invariant... locations vary by RAM Mode#
define symbol RAM_BANK0_SIZE   = 16K;
define symbol RAM_BANK1_SIZE   = 12K;
define symbol RAM_BANK2_SIZE   =  4K;
define symbol RAM_BANK3_SIZE   = 16K;
define symbol RAM_BANK4_SIZE   = 16K;
define symbol RAM_BANK5_SIZE   = 32K;
define symbol RAM_BANK6_SIZE   = 16K;
define symbol RAM_BANK7_SIZE   = 16K;

//MODE0 0kB CACHE 32kB ISRAM 96kB DSRAM
if(USER_SRAM_MODE == 0)
{
	// ISRAM
	define symbol RAM_BANK1 = 0x10000000;
	define symbol RAM_BANK7 = 0x10003000;
	define symbol RAM_BANK2 = 0x10007000;

	// DSRAM
	define symbol RAM_BANK0 = 0x20000000;

	define symbol RAM_BANK3 = 0x20040000;
	define symbol RAM_BANK4 = 0x20044000;
	define symbol RAM_BANK5 = 0x20048000;
	define symbol RAM_BANK6 = 0x20050000;

	define region iRAM  = mem:[from RAM_BANK1 size (RAM_BANK1_SIZE + RAM_BANK7_SIZE + RAM_BANK2_SIZE)];
	define region dRAM1 = mem:[from RAM_BANK0 size (RAM_BANK0_SIZE) ];
	define region dRAM2 = mem:[from RAM_BANK3 size (RAM_BANK3_SIZE + RAM_BANK4_SIZE + RAM_BANK5_SIZE + RAM_BANK6_SIZE) ];
}

//MODE1 4kB CACHE 28kB ISRAM 96kB DSRAM
else if(USER_SRAM_MODE == 1)
{
	// ISRAM
	define symbol RAM_BANK1 = 0x10000000;
	define symbol RAM_BANK7 = 0x10003000;

	// DSRAM
	define symbol RAM_BANK0 = 0x20000000;

	define symbol RAM_BANK3 = 0x20040000;
	define symbol RAM_BANK4 = 0x20044000;
	define symbol RAM_BANK5 = 0x20048000;
	define symbol RAM_BANK6 = 0x20050000;

	define region iRAM  = mem:[from RAM_BANK1 size (RAM_BANK1_SIZE + RAM_BANK7_SIZE)];
	define region dRAM1 = mem:[from RAM_BANK0 size (RAM_BANK0_SIZE) ];
	define region dRAM2 = mem:[from RAM_BANK3 size (RAM_BANK3_SIZE + RAM_BANK4_SIZE + RAM_BANK5_SIZE + RAM_BANK6_SIZE) ];
}

//MODE2 0kB CACHE 0kB ISRAM 128kB DSRAM
else if(USER_SRAM_MODE == 2)
{
	// ISRAM

	// DSRAM
	define symbol RAM_BANK0 = 0x20000000;
	define symbol RAM_BANK1 = 0x20004000;
	define symbol RAM_BANK2 = 0x20007000;

	define symbol RAM_BANK3 = 0x20040000;
	define symbol RAM_BANK4 = 0x20044000;
	define symbol RAM_BANK5 = 0x20048000;
	define symbol RAM_BANK6 = 0x20050000;
	define symbol RAM_BANK7 = 0x20054000;

	define region iRAM  = mem:[from 0 size 0];
	define region dRAM1 = mem:[from RAM_BANK0 size (RAM_BANK0_SIZE + RAM_BANK1_SIZE + RAM_BANK2_SIZE) ];
	define region dRAM2 = mem:[from RAM_BANK3 size (RAM_BANK3_SIZE + RAM_BANK4_SIZE + RAM_BANK5_SIZE + RAM_BANK6_SIZE + RAM_BANK7_SIZE) ];
}

//MODE3 4kB CACHE 0kB ISRAM 124kB DSRAM
else if(USER_SRAM_MODE == 3)
{
	// ISRAM

	// DSRAM
	define symbol RAM_BANK0 = 0x20000000;
	define symbol RAM_BANK1 = 0x20004000;

	define symbol RAM_BANK3 = 0x20040000;
	define symbol RAM_BANK4 = 0x20044000;
	define symbol RAM_BANK5 = 0x20048000;
	define symbol RAM_BANK6 = 0x20050000;
	define symbol RAM_BANK7 = 0x20054000;

	define region iRAM  = mem:[from 0 size 0];
	define region dRAM1 = mem:[from RAM_BANK0 size (RAM_BANK0_SIZE + RAM_BANK1_SIZE) ];
	define region dRAM2 = mem:[from RAM_BANK3 size (RAM_BANK3_SIZE + RAM_BANK4_SIZE + RAM_BANK5_SIZE + RAM_BANK6_SIZE + RAM_BANK7_SIZE) ];
}

// ROM regions
define region ROM_PAGE0_INTVEC              = mem:[from FLASH size (START_OF_SEC_HDR - FLASH)];
define region START_OF_PAGE0_REGION         = mem:[from (PAGE0_ROM_START) size (FLASH_PAGE_SIZE - PAGE0_ROM_START)];
define region ROM_REGION                    = mem:[from (FLASH + FLASH_PAGE_SIZE) size (FLASH_SIZE - FLASH_PAGE_SIZE)];

place at address mem: START_OF_SEC_HDR        { readonly section .security_options };

// C-Runtime blocks
define block CSTACK with alignment = 8, size = __ICFEDIT_size_cstack__ { };
define block HEAP   with alignment = 8, size = __ICFEDIT_size_heap__   { };


// Flash Page0 contains an optional checksum block, as verified by the boot kernel at startup.
// If generating a checksum ("Checksum" linker dialogue box) during the build, it is also
// required to add "--keep __checksum" to the linker "Extra Options" dialogue to preserve the
// linker-generated "__checksum" symbol.
define block CHECKSUM      with alignment = 4, size = 4 { ro section .checksum };

// force mandatory placement of the CHECKSUM block within Page0
place at address 0x000007FC { block CHECKSUM };


// KEEP these blocks, avoiding linker elimination...
keep {
    block CHECKSUM,
};


// initializations...
do not initialize                                { section .noinit };

// expand encoded initialized data variables from flash image into RAM during C-Runtime Startup
initialize by copy                               { rw };

//initialize by copy with packing = none         { section __DLIB_PERTHREAD }; // Required in a multi-threaded application

// ROM: place IVT at start of flash, page zero (ahead of the "meta-data")
place at start of ROM_PAGE0_INTVEC               { ro section .intvec };
place in  START_OF_PAGE0_REGION                  { ro section Page0_region };

// ROM: place remaining read-only code/data in flash, starting at flash page1
place in          ROM_REGION                     { ro };

// place data and stack in lower, always-retained DSRAM region
place in          dRAM1    { rw };
place at end of   dRAM1    { block CSTACK };

// place heap in upper DSRAM region
place in          dRAM2    { block HEAP };

// ISRAM section for placing code in SRAM
place in          iRAM     { section ISRAM_REGION };

initialize by copy { section ISRAM_REGION };

I want to increase __ICFEDIT_size_cstack__  to 80 k and HEAP to 2k. But compilator gives me an section placement errors.

How should i do this correctly?

Top Replies

    •  Analog Employees 
    Feb 14, 2019 +2 verified

    Hello mappy89,

    The STACK size of 80k can't be allocated in the dRAM1 region as it only has a size 16K.

    Since you swapped the sizes of the STACK and HEAP, what you can do is also swap the regions where…