MDK-ARM Microcontroller Development Kit v5.00 and later versions require that support for a particular device must be installed as a separate step from the compilation tool-chain.
This has the benefit of reducing the overall download size and allowing easier updates in the future.
Support for the Analog Devices Microcontroller family of devices in MDK-ARM can be found in the legacy support downloads from Keil.
Additional steps as outlined below are now necessary to get access to the Microcontroller support.
These steps should be performed after the main MDK-ARM compilation tool chain has been downloaded and installed.
Visit the following Keil page and install the required support.
http://www2.keil.com/mdk5/legacy
To install support for the ADuC7xxx ARM7TDMI and ARM7TDMI-S based Microcontrollers, it is necessary to download and install the Legacy Support for ARM7 and ARM9 from the above link.
To install support for the ADuCMxxx Cortex-M3 based Microcontrollers, it is necessary to download and install the Legacy Support for Cortex-M Devices from the above link.