Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.
1. What are the possible input sources for the CRC block?
>> The CRC accelerator can be used to compute CRC for a block of memory locations in the SRAM, flash, or any combination of memory mapped registers.
2. Is there any restriction on the input data size?
>> Yes. CRC works on 32-bits data words only. For data words less than 32-bit, the processor has to pack the data into 32-bit data units
3. Is the CRC polynomial programmable?
>> No. The CRC polynomial is always x32 + x26 + x23 + x22 + x16 + x12 + x11 + x10 + x8 + x7 + x5 + x4 + x2 + x + 1
4. How many processor cycles are needed by the CRC block for one computation?
>> The accelerator takes two clock cycles to compute CRC for one data item. The processor can send one data item for every two clock cycles. therefore, the Cortex-M3 does not need to wait between data transfers to the CRC accelerator.