Q. What is the reference clock for the GP Timers?
A:
Q. What are the operating modes available with the timers?
A: The timers can operate in Free running or periodic mode. In free running mode, the counter increments/decrements from the minimum/maximum value until full/zero scale and starts again. In periodic mode, it starts from the value in the GPTLD MMR until zero/full scale.
The timers also provide PWM function and can also capture 16 interrupt event functions.