Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

CN0300: Power Consumption

What is the power consumption of the ADuCM360?

 

When operating normally, the entire circuit consumes 2.25 mA typically. When
held in a reset state, the entire circuit consumes less than 600 μA.  For
further details on power consumption of the ADuCM360, see AN-1111.

http://www.analog.com/static/imported-files/application_notes/AN-1111.pdf
Comments
Anonymous
Related