Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

CN0300: Is it possible to use the ADuCM361 instead of the ADuCM360?

For CN0300, could the ADuCM361 be used – in other words implement the
temperature readings and DAC feedback control with just one ADC instead of 2?

 

As the circuit is currently built, if one ADC is used for everything, the DAC
output voltage is not stable. The instability occurs when AIN9 is
enabled/disabled as the ADC input channel. When this change occurs, the input
impedance on AIN9 changes due to switches on the input MUX being turned off/on.

When AIN9 is always selected as the input to AIN0 as is the case for this
ADuCM360 implementation, this is not an issue.
Comments
Anonymous
Related