Post Go back to editing

Eval-ADuCM355 Interrupts in sample code are never executing

Category: Software
Product Number: ADuCM355
Software Version: aducm355-examples

Hey,

i'm trying to test the functionalities of the aducm355 with the code examples. I haven't modified the code in any way.

I tried the following code examples:

- Temperatur

- Impedance (for this sample i connected some resistors on the interface)

An interrupt should occur and data should be printed out, but as soon as the function "AD5940_GetMCUIntFlag()" get called the return value stays 0 all the time. So i guess the interrupt never occurs? 

Is this behaviour intended?  Do i have to modifiy the example code so the interrupt get executed? 

Thanks for any help

Shaheen

Thread Notes

Moved from Ultra Low Power Microcontrollers to Precision Microcontrollers on Monday, November 20, 2023 5:24:07 AM by BryanD