Post Go back to editing

ADIChip.ini for ADuCM362/3 is needed

Category: Choose a category
Product Number: ADucm362/3 serial loader
Software Version: cm3wsd version 2

In previous thread, https://ez.analog.com/analog-microcontrollers/precision-microcontrollers/f/discussions/18624/aducm362-adichip-ini-file, it listed a directory to download the cm3wsd, but the link is no longer available.

Can you update me?

I am working with ADuCM362/3 to replace ADuCM360/1

I downloaded cm3wsd from https://ez.analog.com/analog-microcontrollers/precision-microcontrollers/m/file-uploads/348, but when i try to flash it, it ran into an error:



add more info
[edited by: dinrail at 3:15 PM (GMT -4) on 31 Aug 2022]
Parents
  • Hi,

    If you go to the folder where CM3WSD is installed you will see an ADIChip.ini file.

    Can you try to copy and paste the [ADuCM360] and [ADuCM361] sections and rename these new sections as [ADuCM362] and [ADuCM363] so it looks like the screenshot below?

    If that works, then you can modify the ROMEnd and RAMEnd to match the particular memory sizes of the silicon you are using..

    Best regards,

    Raquel

  • Further testing seems to indicate another problem:

    I am using CM3WSD ver 2.0, 2012

    I added the entry for ADIChip.ini as you instructed

    When I flash it, cm3wsd indicating page of 512 bytes, but the data sheet for ADuCM362 says the page size is 2K, it doesn't seem right to me



Reply Children
No Data