Hello,
I have been testing the Cyclic Voltammetry code located in here using the ADuCM355 Evaluation Board.
At some point I want to use the external RTIA of the LPTIA, but in order to do that I need to access the RC0_0 and RC0_1 pins physically to connect the external resistor. However, those two pins cannot be accessed on the Evaluation Board, unless I am missing something.
- Is there any technique to access those two pins physically that I am not aware of?
- Or alternatively, do you count on any version of the code that uses a HSTIA so I can connect the resistor to DE0 and AIN0 pins which are accessible on the Evaluation Board?
Thank you!