Aducm360 while reflashing it shows the error check aducm jlnk id it fails ,and register string 0x40004024 not found error cames
Aducm360 while reflashing it shows the error check aducm jlnk id it fails ,and register string 0x40004024 not found error cames
Hi,
Have you verified the JLink via JLink commander?
Example:
SEGGER J-Link Commander V6.98a (Compiled Mar 5 2021 17:02:18)
DLL version V6.98a, compiled Mar 5 2021 17:01:02
Connecting to J-Link via USB...O.K.
Firmware: J-Link Lite-ADI Rev.1 compiled Jan 7 2013 17:58:04
Hardware version: V1.00
S/N: 541006197
OEM: ADI
VTref=3.592V
Type "connect" to establish a target connection, '?' for help
J-Link>connect
Please specify device / core. <Default>: ADUCM362
Type '?' for selection dialog
Device>ADUCM360
Please specify target interface:
J) JTAG (Default)
S) SWD
T) cJTAG
TIF>SWD
Specify target interface speed [kHz]. <Default>: 4000 kHz
Speed>
Device "ADUCM360" selected.
Connecting to target via SWD
Found SW-DP with ID 0x2BA01477
DPv0 detected
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x412FC231. Implementer code: 0x41 (ARM)
Found Cortex-M3 r2p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB000 SCS
ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT
ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB
ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM
ROMTbl[0][4]: E0040000, CID: B105900D, PID: 003BB923 TPIU-Lite
ROMTbl[0][5]: E0041000, CID: B105900D, PID: 003BB924 ETM-M3
Cortex-M3 identified.
J-Link>
While reflashing the code,
The log below will be obtained( if using EVALADICUP360 and USB cable connected to User port on the board):
Tue Jan 11, 2022 00:48:16: IAR Embedded Workbench 8.50.6 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\bin\armproc.dll)
Tue Jan 11, 2022 00:48:16: Download complete.
Tue Jan 11, 2022 00:48:16: Loaded debugee: ..........\EVAL-ADICUP360-master\projects\ADuCM360_demo_blink\IAR\Release\
Exe\ADuCM360_demo_blink.out
Tue Jan 11, 2022 00:48:17: Target reset