What's the actual ADC sampling rates of AD5940 and ADUCM355, and how to make a choice?

Hello,

The first Q:

  The ADC sampling rates of these two products, AD5940 and ADUCM355, are both inconsistent in the datasheet. The feature overview, specification part and the detail introduction of ADC module offer different data. What is the exact value?(normal mode and high speed mode)

 Screenshot from datasheet or hardware reference

    ADUCM355:

              

             

               

    AD5940:

                

               

                 

The second Q:

  What are the advantages of EVAL-AD5940 and EVAL-ADUCM355, respectively. Can I use an additional MCU to control ADUCM355? Which should I choose?

  • Hi BlingBling,

    The sampling rate of the ADC depends on the configuration you choose for the digital filters that perform post processing. The 800k samples per second specification indicates this is available with no filtering.

    The 400 kSPS and 200 kSPS specification are when the Sinc3 filter is enabled with an OSR of 4 (I assume four samples are low-passed with an FIR/IIR into a single value). This is the "decimation factor" to the right of the BASIC ADC SPECIFICATIONS.

    Each functional block may impact your actual sample rate. I recommend profiling interrupts, or the time it takes to fill up the FIFO to verify sampling rates for your settings.

    To answer your second question, the ADuCM355 has an integrated Cortex-M3 processor. The AD5940 is just an analog front end, bring your own micro.

    Best,

    Matt

  • Thanks for your answer,

    What about the choice between EVAL-AD5940 and EVAL-ADUCM355? I think ADUCM355 has better performance and integration. However, EVAL-AD5940 is much more expensive than EVAL-ADUCM355. What‘s the cause?

  • Hi,

    The eval-AD5940 kit comes with EVAL-ADICUP3029 base board (containing microcontroller for testing and verification), hence the cost.