Post Go back to editing

AD5934 - Conductivity Probe (K = 1, TDS - 0 to 10,000)

Hi,

  1. We have a plan to implement AD5934 in our new project for Conductivity Probe K =1 so Is it suit for us..?
  2. May I know the Lifetime of these IC's..?
  3. Can we connect the conductivity probe of K = 10 in AD5934 ..? and
  4. May I know the probe range and maximum TDS Value for AD5934..?
  5. May I know the year (invention) of AD5934 AND ad5940..?
  6. Is there any updated IC available over AD5934...?
  7. Is it the right choice, when we use this Ic's AD5940 alternate for AD5934...?