ADuCM355 Hardware Reference Manual (UG-1262) error?

Hi All,

The LPTIACON0 description gives bit 0 as:

In case this is not legible, this says:

Bits    Bit name      Description

0        TIAPDEN      TIA Power Down. LPTIA0 power-down control bit.
                              0 Power up.
                              1 Power down

Whilst the description for LPTIACON1 gives bit 0 as:

Again, in case this is not legible, this says:

Bits    Bit name      Description

0        TIAPDEN      Current Boost Control
                              0 Normal mode.
                              1 Increase amplifier output stage current to quickly charge external capacitor load. Intended for use with high current sensors like oxygen electrochemical sensor.

Is the description for bit 0 in LPTIACON1 correct? If it is correct, then what is the relationship between this bit and bits [4:3} IBOOST (Current Boost Control).

Or should LPTIACON1 bit 0 be TIA Power Down like LPTIACON0?

Thanks!