What are the differences between these two microcontrollers. The only documented differences seem to be: more SRAM, more flash, one extra UART? Are there more differences between these devices and is it recommended to use the ADuCM362 as a replacement in new designs? Are there plans to fully support the 362 in CrossCore and include the full example set in the CMSIS pack? Right now it looks like there would be some advantages to targeting this device instead of the 360 for my project but the documentation and support seem far less mature despite the 362 being several years old. Can anyone offer recommendations?
Hi Mike,
Besides what you mentioned, some key points of differences as below:
1. when PGA =1, the buffer can be enabled. ADUCM360 can not.
2. Optimization on clock. A little difference on the clock related…
Hi,
For ADuCM362 also,
The difference between AVDD and IOVDD must be ≤0.3 V.
Regards,
Akila