CN0359 code compatibility for ADuCM362

Hi

Can I replace the ADuCM360 to the ADuCM362 in CN0359 without code modification ? Only difference in my application is that im not using SPI LCD.

Best Regards

KoRba

Parents
  • +1
    •  Analog Employees 
    on Jan 7, 2019 7:28 PM over 1 year ago

    Hi KoRba,

    You should be able to replace the ADuCM360 with the ADuCM362 in the CN0359.  Both devices should function exactly the same.  The only thing that you might have to do is just ensure that the pin definitions in the code match what is on the board.   Especially the UART because the ADuCM362 has two unique UART peripherals where the ADuCM360 only has 1 (even know that one UART is pinned out on 2 sets of pins via a switch.)

    Cheers,

    Brandon

Reply
  • +1
    •  Analog Employees 
    on Jan 7, 2019 7:28 PM over 1 year ago

    Hi KoRba,

    You should be able to replace the ADuCM360 with the ADuCM362 in the CN0359.  Both devices should function exactly the same.  The only thing that you might have to do is just ensure that the pin definitions in the code match what is on the board.   Especially the UART because the ADuCM362 has two unique UART peripherals where the ADuCM360 only has 1 (even know that one UART is pinned out on 2 sets of pins via a switch.)

    Cheers,

    Brandon

Children