Hello,
Congratulations releasing ADICUP360.
I have been trying to use ADICUP360 with following wiki information but encounter an error.
(I try to test blink project and GDB OPEN OCD debugger as following on Wiki instruction)
Eclipse fail to download elf file with error message as below.
Open On-Chip Debugger 0.10.0-dev-00025-g81cc011-dirty (2015-08-17-13:23)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'swd'
adapter speed: 5000 kHz
adapter_nsrst_delay: 100
cortex_m reset_config vectreset
Error: unable to find CMSIS-DAP device
This error seems Eclipse cannot recognize ADICUP360 via USB port. (Because when I unconnected ADICUP360 with PC, Eclipse show the same error message as above.)
I suppose I miss something setting on ADICUP360 board.. But I can not figure out where is wrong...
Jumper and DIP SW setting are default.
I've tried also another ADICUP360 and other USB port and cable and several S1-S4 switch combinations but all fail.
I would appreciate if you have any suggestions.
Best regards,
Sofy
I've tried to setup ADICUP360 to another PC.
There is no issue, very success to connect ADICUP360 and run.
So the problem is my PC...not ADICUP360 Eclipse or mbed driver.
Thank you for your advice.