Hello,
Congratulations releasing ADICUP360.
I have been trying to use ADICUP360 with following wiki information but encounter an error.
(I try to test blink project and GDB OPEN OCD debugger as following on Wiki instruction)
Eclipse fail to download elf file with error message as below.
Open On-Chip Debugger 0.10.0-dev-00025-g81cc011-dirty (2015-08-17-13:23)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'swd'
adapter speed: 5000 kHz
adapter_nsrst_delay: 100
cortex_m reset_config vectreset
Error: unable to find CMSIS-DAP device
This error seems Eclipse cannot recognize ADICUP360 via USB port. (Because when I unconnected ADICUP360 with PC, Eclipse show the same error message as above.)
I suppose I miss something setting on ADICUP360 board.. But I can not figure out where is wrong...
Jumper and DIP SW setting are default.
I've tried also another ADICUP360 and other USB port and cable and several S1-S4 switch combinations but all fail.
I would appreciate if you have any suggestions.
Best regards,
Sofy
Sorry for my late response.
I've tried again the setup from scratch with connected ADICUP360 entire setup steps.
But situation is not change. (even MBED driver bundled in ADuCM360-IDE is successfully installed)
I will try to setup another PC.