[ADICUP360]encounter an error message "unable to find CMSIS-DAP device".

Hello,

Congratulations releasing ADICUP360.

I have been trying to use ADICUP360 with following wiki information but encounter an error.

(I try to test blink project and GDB OPEN OCD debugger as following on Wiki instruction)


Eclipse fail to download elf file with error message as below.


Open On-Chip Debugger 0.10.0-dev-00025-g81cc011-dirty (2015-08-17-13:23)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.org/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'swd'

adapter speed: 5000 kHz

adapter_nsrst_delay: 100

cortex_m reset_config vectreset

Error: unable to find CMSIS-DAP device

This error seems Eclipse cannot recognize ADICUP360 via USB port. (Because when I unconnected ADICUP360 with PC, Eclipse show the same error message as above.)

I suppose I miss something setting on ADICUP360 board.. But I can not figure out where is wrong...

Jumper and DIP SW setting are default.

I've tried also another ADICUP360 and other USB port and cable and several S1-S4 switch combinations but all fail.

I would appreciate if you have any suggestions.

Best regards,

Sofy

Parents
  • 0
    •  Analog Employees 
    on Feb 16, 2016 7:52 PM over 4 years ago

    Hi Sofy,

    Please make sure that you have jumpers J3 and J4 shorted, and that you are connected to the DEBUG USB port on the ADICUP360.

    I'm wondering if the device driver for the USB port you are using wasn't properly installed.  It is important during the installation of the Eclipse IDE that the MBED drivers are completely installed before moving onto the next step.

    Do you remember skipping over this step?  Or a prompt saying that the drivers were unsuccessful and instead of trying again, you may have moved forward?

    Could you try connecting the DEBUG USB to a different USB port on your PC, and letting all the drivers completely install before using the Eclipse program?   If that doesn't work, it might be best to try and uninstall the software and try again.

    Keep me posted

Reply
  • 0
    •  Analog Employees 
    on Feb 16, 2016 7:52 PM over 4 years ago

    Hi Sofy,

    Please make sure that you have jumpers J3 and J4 shorted, and that you are connected to the DEBUG USB port on the ADICUP360.

    I'm wondering if the device driver for the USB port you are using wasn't properly installed.  It is important during the installation of the Eclipse IDE that the MBED drivers are completely installed before moving onto the next step.

    Do you remember skipping over this step?  Or a prompt saying that the drivers were unsuccessful and instead of trying again, you may have moved forward?

    Could you try connecting the DEBUG USB to a different USB port on your PC, and letting all the drivers completely install before using the Eclipse program?   If that doesn't work, it might be best to try and uninstall the software and try again.

    Keep me posted

Children
No Data