Post Go back to editing

ADuCM360 How To Enable SysTick_Handler


Hi all,

I have an issues with ADuCM360, can you please point me ?

I want to enable SysTick_Handler interrupt, this function in exception_handlers.c file

I'm trying to build CN0359 source code with ADuCM360 IDE(C++ project).

How can i enable it ?

Thanks !

Parents
  • Hi

    The SysTick_Handler is already added in interrupt vector table from vectors_ADuCM360.c file. In exceptions_handle.c file it is defined as "weak" function which means that you can redefine it in your code.

    If you will use "Hello World" template you will have an example how this interrupt routine is used inside of the Timer.cpp file.

Reply
  • Hi

    The SysTick_Handler is already added in interrupt vector table from vectors_ADuCM360.c file. In exceptions_handle.c file it is defined as "weak" function which means that you can redefine it in your code.

    If you will use "Hello World" template you will have an example how this interrupt routine is used inside of the Timer.cpp file.

Children
No Data