Post Go back to editing

How to use a J-LINK with ADICUP360

I have been working with the ADICUP360. Awesome tool! I have progressed to where I need to connect the board to my J-LINK probe and am having trouble. I see from the schematics that the 10-pin Cortex debug connector P16 connects to the M360 SWD pins, but also to the on-board SDA interface. How han I force the SDA interface to relinquish contol and allow the J-LINK to control the SWD pins?

Thanks in advance!

Parents
  • Hi Brandon,

    Up and running! Thanks for the help.

    You are correct, the on-board SDA interface relinquishes control of the SWD pins when the Debug USB port is disconnected. When I power the board through the User USB port, the J-Link attached to P16 takes control of the M360 without conflict.

    Regards,

    Steven

Reply
  • Hi Brandon,

    Up and running! Thanks for the help.

    You are correct, the on-board SDA interface relinquishes control of the SWD pins when the Debug USB port is disconnected. When I power the board through the User USB port, the J-Link attached to P16 takes control of the M360 without conflict.

    Regards,

    Steven

Children
No Data