Hello,
I am planning on using the ADuC702x MCU for an application (aduc7022 specifically, first time using this mcu).
I expect an analog input from the range of 0V - 3.3V. However I see that the ADuC702x has an internal 2.5V Vref, reference voltage for its ADC.
The datasheet sheet states that the band gap reference (which I assumer means 0V-Vref) can be changed from the 2.5V from an external reference.
Does this simply mean I can route 3.3V to the Vref pin (pin 33), program REFCON = 0x00, and I should be able to use the ADC for a range from 0V-3.3V?