Post Go back to editing

ADuc7020

Category: Software
Product Number: AduC7020
Software Version: Keil&ARMSWD

We purchased the development board component Aduc7020 from ADI Company, and the serial download software ARMSWD was used for the subsequent download program. According to the official document for the key reset operation, download, but found that ARMSWD can not recognize the chip, can not write the program.

After repeated attempts, I found that the development board component was always running in the previous DEMO example, which was explained as follows:

{

Description   : Uses Potentiometer on the ADuC7023 part.

                           Potentiometer controls the voltage to ADC0 chennel.

                            Internal measurement of ADC0 via ADC is replicated

                            on DAC1 output. This has the affect of controlling the

                            brightness of the LED, D1.

                            Ensure "POT" and "DAC" switches of S1 are "On"

 Demo.zip

}

 

I have been unable to update the program I wrote.

Here is how my circuit is connected

what's wrong with our schematic,can you give me some suggestion,thanks.

Parents
  • Hi Jeffrey,

    Have you changed the configuration of the ARMWSD, such as the selected part, serial port, and baud rate?

    The key reset operation you mentioned, did you mean the sequence below?

    You must press and hold the serial download button, then press and hold the reset button.

    After that, release the reset button, then the serial download button.

    Regards,

    Karl

  • Dear Karl,

    ARMSWD displays the following screen after you perform the key operations(

    press and hold the serial download button, then press and hold the reset button.

    After that, release the reset button, then the serial download button.) described above.

    Then continue to press the reset button as the ARMSWD prompted, and the following screen will appear.

    I consulted the relevant forum, and the discussant said THE above showed no chip found.

    I have been searching for this reason for several days, but I cannot find out what is wrong. Can you give me some other suggestions?

    Best Regards,

     

    Jeffrey

  • Hi Jeffrey,

    The image you sent does show that ARMWSD detected ADuC7020, but the configuration in the ARMWSD may not have been set to the correct part.

    Have you checked the configuration to see if ADuC7020 is properly selected?

    Once you perform the key operation above and press "Start" in the ARMWSD, you don't need to press the reset button again.

    Regards,

    Karl

Reply
  • Hi Jeffrey,

    The image you sent does show that ARMWSD detected ADuC7020, but the configuration in the ARMWSD may not have been set to the correct part.

    Have you checked the configuration to see if ADuC7020 is properly selected?

    Once you perform the key operation above and press "Start" in the ARMWSD, you don't need to press the reset button again.

    Regards,

    Karl

Children