ADuC702x temperature sensor

how to calculate the temperature from the on-chip sensor ADC reading?

Parents
  • 0
    •  Analog Employees 
    on Jul 8, 2010 3:43 PM

    The ADuC702x has an on-chip temperature sensor. This sensor can be used to indicate the die temperature of the part. Its accuracy is typically +/-3 degree C. its reading at 25degree C is 780mV typical with a temperature coefficient of -1.3mV/degree C.

    Therefore temperature can be calculated using the formula:

    Temperature = (812.5-ADC reading in mV)/1.3

    The LSB weight of the ADC is 2.5V/2^12 or 610uV. 780mV at 25deg C correspond to 812.5mV at 0deg C.

    V = -1.3 x Temp /1000 + 812.5 mV

    812.5mV is 0x533 hex

    An equivalent formula is:

     

    Temperature = 0x533 – Sensor Voltage) / 1.3

Reply
  • 0
    •  Analog Employees 
    on Jul 8, 2010 3:43 PM

    The ADuC702x has an on-chip temperature sensor. This sensor can be used to indicate the die temperature of the part. Its accuracy is typically +/-3 degree C. its reading at 25degree C is 780mV typical with a temperature coefficient of -1.3mV/degree C.

    Therefore temperature can be calculated using the formula:

    Temperature = (812.5-ADC reading in mV)/1.3

    The LSB weight of the ADC is 2.5V/2^12 or 610uV. 780mV at 25deg C correspond to 812.5mV at 0deg C.

    V = -1.3 x Temp /1000 + 812.5 mV

    812.5mV is 0x533 hex

    An equivalent formula is:

     

    Temperature = 0x533 – Sensor Voltage) / 1.3

Children
No Data